FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Installation necessity of a DC reactor
FAQ
Installation necessity of a DC reactor
What is the condition where a DC reactor connection is required?
- Category :
Answer
A DC reactor connection is required under the following conditions.
- Inverter capacity is 75K or higher - Motor capacity is 75 kW or higher. If any of the above conditions is met, always connect a DC reactor.
- Inverter capacity is 75K or higher - Motor capacity is 75 kW or higher. If any of the above conditions is met, always connect a DC reactor.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800, option