Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21089
  • Release Date : 2018/08/22 16:25
  • Print

Wiring length

In the FR-A700/F700P, the maximum wiring length is 100 m when the shielded cable is used. Is it changed in the FR-A800/F800?
Category : 

Answer

In the FR-A800/F800, the restriction on the wiring length of the shielded cable is eliminated. The wiring length is up to 500 m as is the case with the unshielded cable.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries