FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Vector control
FAQ
Vector control
Under Vector control (speed control), why does the E.OSD speed deviation excess detection occur even the setting value of Pr.285 (Excessive speed deviation detection frequency) is "9999"?
- Category :
Answer
"E.OSD" occurs when the rotation speed is not decreased for one second despite the start command (STF, STR) is turned OFF.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700