FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Torque limit
FAQ
Torque limit
When performing the torque limit of the speed control, are Pr.816 (Torque limit level during acceleration) and Pr.817 (Torque limit level during deceleration) valid if Pr.815 (Torque limit level 2) is set, TL (torque limit selection) signal is turned ON, and the second torque limit is used?
- Category :
Answer
When the second torque limit is used, the settings of Pr.816 and 817 are valid.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700