FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Connection cable of FR-Configurator
FAQ
Connection cable of FR-Configurator
Can I connect FR-Configurator (FR-SW3-SETUP-WJ) with a standard USB connector (B connector)?
- Category :
Answer
The following USB connectors are available.
For FR-A700: USB B connector (B receptacle)
For FR-E700: USB Mini-B connector (Mini-B receptacle)
Use the USB cable suitable for the connector type.
The recommended cable connected to the Mini-B connector is MR-J3USBCBL3M.
For FR-A700: USB B connector (B receptacle)
For FR-E700: USB Mini-B connector (Mini-B receptacle)
Use the USB cable suitable for the connector type.
The recommended cable connected to the Mini-B connector is MR-J3USBCBL3M.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700