FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Brake resistor
FAQ
Brake resistor
It is described that the high-duty brake resistor FR-ABR cannot be installed to the FR-E700-0.1K/0.2K. Can I install the brake unit?
- Category :
Answer
The brake unit can be installed.
FR-BU2-1.5K and GZG300W50 ? can be used in combination.
FR-BU2-1.5K and GZG300W50 ? can be used in combination.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ