FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Offline auto tuning
FAQ
Offline auto tuning
When offline auto tuning completes, the setting value of Pr.96 (Auto tuning setting/status) becomes "3". Should I change this setting when performing the actual operation?
- Category :
Answer
Leave the setting of Pr.96 as "3".
It indicates that auto tuning has been completed and the motor constant has been read.
When it is changed unnecessarily, the constant of auto tuning will not be used.
It indicates that auto tuning has been completed and the motor constant has been read.
When it is changed unnecessarily, the constant of auto tuning will not be used.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700