FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Do you have a sample program for 485 communication?
FAQ
Do you have a sample program for 485 communication?
I am planning to operate the FR-E500 from the programmable controller via RS485 communication.
Do you have a sample program to do this using the MELSEC-A or FX on the programmable controller?
Do you have a sample program to do this using the MELSEC-A or FX on the programmable controller?
- Category :
Answer
We do not offer a sample program for the programmable controller.
Refer to the Instruction Manual and create the program by yourself.
Refer to the Instruction Manual and create the program by yourself.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Others
- Series
- FR-E500