FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Regenerative driving capability
FAQ
Regenerative driving capability
How much is the regenerative driving capability?
- Category :
Answer
Continuous 100% regenerative braking torque is available for the rated capacity of the high power factor converter. (The same braking ability of the FR-A201 inverter with the built-in power supply regenerative function is achieved.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- High power factor converter
- Series
- Option