FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Are conventional parameter units still available?
FAQ
Are conventional parameter units still available?
Are the conventional parameter units (FR-PU01, PU02, and PU03) still available?
- Category :
Answer
The key sheet fixed to the inverter is used for operation.
Therefore, the conventional parameter unit cannot be used. (There is no connector to connect it.)Only the PU operation type allows for using the FR-PU03.
Therefore, the conventional parameter unit cannot be used. (There is no connector to connect it.)Only the PU operation type allows for using the FR-PU03.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Common
- Series
- FR-U100