FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > What applications are suitable?
FAQ
What applications are suitable?
What applications are suitable?
- Category :
Answer
Variable speed control of small-capacity motor and other applications for which small size and low cost are required.
(Examples: Replacement for gears and pulleys, contactless version of reversible contactor, standardization of machines in 50/60 Hz area, agricultural machine, conveyor, ventilation fan)The inverter can be used in an area where only the single-phase power supply is available.
(Examples: Replacement for gears and pulleys, contactless version of reversible contactor, standardization of machines in 50/60 Hz area, agricultural machine, conveyor, ventilation fan)The inverter can be used in an area where only the single-phase power supply is available.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Common
- Series
- FR-U100