FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-PA07
FAQ
FR-PA07
By connecting the optional FR-PA07, can I use both the inverter operation panel and FR-PA07?
- Category :
Answer
Basically it is not possible due to the operation command source.
However, if Pr.77 (Parameter write selection) is set to "2", you can use both the FR-PA07 and the inverter operation panel to set parameters.
Note that you can switch between forward and reverse rotation from the FR-PA07 only.
However, if Pr.77 (Parameter write selection) is set to "2", you can use both the FR-PA07 and the inverter operation panel to set parameters.
Note that you can switch between forward and reverse rotation from the FR-PA07 only.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ