FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-PA07
FAQ
FR-PA07
I am using the optional operation panel FR-PA07 connected with a cable with Pr.79 (Operation mode) set to "3".
When using this FR-PA07 and external terminals, does the "RUN" key on the FR-PA07 work?
When using this FR-PA07 and external terminals, does the "RUN" key on the FR-PA07 work?
- Category :
Answer
No. The "RUN" key on the FR-PA07 does not work.
The start command is accepted from the external source.
The start command is accepted from the external source.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ