FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-Configurator
FAQ
FR-Configurator
Can I connect a single instance of the FR-Configurator (FR-SW3-SETUP-WJ) setup software to multiple inverters via USB?
- Category :
Answer
No. You cannot connect it to multiple inverters.
You can only connect a single personal computer to a single inverter via USB.
You can only connect a single personal computer to a single inverter via USB.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700