FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Parameter setting
FAQ
Parameter setting
Can I perform forward and reverse operations with the RUN key on the panel only with parameter setting and without using signals from the external terminal of the inverter?
- Category :
Answer
You can perform forward and reverse operations with the RUN key on the operation panel by setting Pr.40 (RUN key rotation direction selection).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ