FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Operation panel (FR-PA02)
FAQ
Operation panel (FR-PA02)
When using the operation panel (FR-PA02) for FR-E500 with other inverters, how should I set Pr.146 (Built-in potentiometer switching)?
- Category :
Answer
Set Pr.146 (Built-in potentiometer switching) to "0".
This allows for using the potentiometer built in the FR-PA02 to set the frequency.
(Set this parameter to "1" when the built-in potentiometer is not used.)
This allows for using the potentiometer built in the FR-PA02 to set the frequency.
(Set this parameter to "1" when the built-in potentiometer is not used.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ