FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > CC-Link, analog output card
FAQ
CC-Link, analog output card
Can I use the CC-Link card (FR-A7NC E kit) and the analog output card (FR-A7AY E kit) simultaneously?
- Category :
Answer
You can install only one option card.
If you want to use two types of cards, replace the inverter with the FR-A700 series.
If you can use RS485 communication instead of CC-Link communication, you can connect a single analog output card to the standard PU connector port.
If you want to use two types of cards, replace the inverter with the FR-A700 series.
If you can use RS485 communication instead of CC-Link communication, you can connect a single analog output card to the standard PU connector port.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700