FAQ


FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Saving Data Collecting Servers > Recommended replacement cycle for battery (EcoWebServerIII).
FAQ
Recommended replacement cycle for battery (EcoWebServerIII).
Instruct the recommended cycle for replacing battery of the EcoWebServerIII (MES3-255C-EN, MES3-255C-DM-EN)
Answer
Recommended replacement cycle of the battery (Q6BAT) for the EcoWebServerIII (MES3-255C-EN, MES3-255C-DM-EN)is 3 years. Provided that battery life varies according to energized time ratio as below.
"ERR. LED" of Server section lights upon battery exhaustion. For inquiries on the replacement battery, contact the dealer where you purchased this product.
The backup battery built in the demand control unit of the device with demand control function (MES3-255C-DM-EN) is not replaceable. Where voltage of a battery for clock backup is dropped, consider to update the EcoWebServerIII (MES3-255C-DM-EN). Compensation for power failure for the battery of clock backup is cumulatively 5 years (battery life 10 years).
* Energized time ratio: ratio while power ON of the EcoWebServerIII.
| Energized time ratio | Guaranteed value |
| 0% | 13,700hrs, 1.57years |
| 30% | 19,100hrs, 2.18years |
| 50% | 25,800hrs, 2.96years |
| 70% | 40,000hrs, 4.57years |
| 100% | 43,800hrs, 5years |
"ERR. LED" of Server section lights upon battery exhaustion. For inquiries on the replacement battery, contact the dealer where you purchased this product.
The backup battery built in the demand control unit of the device with demand control function (MES3-255C-DM-EN) is not replaceable. Where voltage of a battery for clock backup is dropped, consider to update the EcoWebServerIII (MES3-255C-DM-EN). Compensation for power failure for the battery of clock backup is cumulatively 5 years (battery life 10 years).
* Energized time ratio: ratio while power ON of the EcoWebServerIII.
- Product Name
- Energy Saving Data Collecting Servers
- Series
- EcoWebServerIII