Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22119
  • Release Date : 2018/08/27 16:41
  • Update : 2018/09/07 11:38
  • Print

Method for measuring a circuit over 600A (EcoMonitorPlus/Light).

Instruct a method for measuring a circuit over 600A using the Energy Measuring Unit (EcoMonitorPlus/Light).
Category : 

Answer

Attach a current transformer (CT) whose secondary current is 5A to the measuring point, then connect a split-type 5A current sensor (Model: EMU-CT5-A, EMU2-CT5, EMU2-CT5-4W) with the secondary side of the CT.
1. In case of EcoMonitorPlus.

 
 
2. In case of EcoMonitorLight.

 
Product Name
Energy Measuring Units
Series
EcoMonitor Plus, EcoMonitorLight

May I have your opinion?

Inquiries