Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22125
  • Release Date : 2018/08/27 16:41
  • Print

Cautions for replacing a battery (Model: EMU4-LM).

Instruct how to handle power supply when replacing a battery of the Logging Unit (Model: EMU4-LM) for the Energy Measuring Unit.
Category : 

Answer

Make sure to power OFF of the EcoMonitorLight or EcoMonitorPlus when replacing a battery of the Logging Unit (Model: EMU4-LM) for the Energy Measuring Unit.
Replacing the battery while power ON may cause electric shock and malfunction.
Note that current time data, logging data and system log data are deleted after replacing the battery.
Output a logging data and system log data into an SD memory card before replacing the battery. Then set time after replacing the battery.
* Since logging ID, logging mode, logging start time, logging cycle of detail data, setting value of logging elements are stored into the nonvolatile memory, they will not be deleted.
Product Name
Energy Measuring Units
Series
EcoMonitor Plus, EcoMonitorLight
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?