Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22126
  • Release Date : 2018/08/27 16:41
  • Print

Setting of "Master / slave setting switch" (Model: EMU4-D65).

An error is indicated immediately after starting the Display Unit (Model: EMU4-D65) for the Energy Measuring Unit.
What kind of causes assumed?
Category : 

Answer

It is assumed that setting of "Master/Slave setting switch" at the bottom of the Display Unit (Model: EMU4-D65) for the Energy Measuring Unit is wrong. Perform settings as below depending on usages.

1. Set "Master (switch 1: OFF, switch 2: OFF)" where one Display Unit is connected to one Energy Measuring Unit.
2. Set one of Display Units as "Master (switch 1: OFF, switch 2: OFF)", other Display Units as "Slave (switch 1: ON, switch 2: OFF)" where plural (Maximum 7 units) Display Units are connected to one Energy Measuring Unit.
Product Name
Energy Measuring Units
Series
EcoMonitor Plus
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?