FAQ


FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > As to simple measuring function of the EcoMonitorPlus (Model: EMU4-BM1-MB、EMU4-HM1-MB、EMU4-A2、EMU4-VA2).
FAQ
As to simple measuring function of the EcoMonitorPlus (Model: EMU4-BM1-MB、EMU4-HM1-MB、EMU4-A2、EMU4-VA2).
How does simple measuring function of EcoMonitorPlus (Model: EMU4-BM1-MB, EMU4-HM1-MB, EMU4-A2, EMU4-VA2) work?
Answer
The function calculates the value of each measurement element of voltage, power factor by inputting only current using setting value.
This function is used when wiring for voltage input is impossible due to installation environment or wiring condition. Refer to "user's manual detailed edition" for each unit as to details like measurement elements.
The manual is downloadable in this site.
This function is used when wiring for voltage input is impossible due to installation environment or wiring condition. Refer to "user's manual detailed edition" for each unit as to details like measurement elements.
The manual is downloadable in this site.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus