FAQ


FAQAbout Products

- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > As to the current sensor usable for the EcoMonitorPlus (Model: EMU4-BM1-MB, EMU4-HM1-MB, EMU4-A2, EMU4-VA2).
FAQ
As to the current sensor usable for the EcoMonitorPlus (Model: EMU4-BM1-MB, EMU4-HM1-MB, EMU4-A2, EMU4-VA2).
Instruct what kind current sensor is usable for EcoMonitorPlus (Model: EMU4-BM1-MB, EMU4-HM1-MB, EMU4-A2, EMU4-VA2).
Answer
Refer to the below table as to current sensor usable for EcoMonitorPlus (Model: EMU4-BM1-MB, EMU4-HM1-MB, EMU4-A2, EMU4-VA2).

*2. It will conform to UL standard, CE marking in combination with the main unit.

*2. It will conform to UL standard, CE marking in combination with the main unit.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus