FAQ


FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > As to logging after removing an SD memory card.
FAQ
As to logging after removing an SD memory card.
Is it impossible to log the data in a state of removing the SD memory card from the EMU4-LM?
Answer
Since the EMU4-LM performs data logging, it is possible to log the data even in a state of removing the SD memory card.
Provided that the period for data logging is specified according to the logging cycle.
Since it deletes data successively from older one when exceeding the specified period, insert the SD memory card within the period to backup data.
Provided that the period for data logging is specified according to the logging cycle.
Since it deletes data successively from older one when exceeding the specified period, insert the SD memory card within the period to backup data.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus, EcoMonitorLight