FAQ
FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Power Management Meters > Electrical Indicators > Replied value on the communication operation test of test mode (ME96SS series).
FAQ
Replied value on the communication operation test of test mode (ME96SS series).
What data are replied on the test mode?
Are the initial set values displayed regardless of setting?
Are the initial set values displayed regardless of setting?
Answer
(A) Measurement values
As for the measurement elements on the test mode screen, the set values are displayed. As for the other measurement elements, 0 is displayed. (1 is displayed for the power factor.)
As for the measurement elements on the test mode screen, the set values are displayed. As for the other measurement elements, 0 is displayed. (1 is displayed for the power factor.)
(B) 16-bit Monitor
The current contact input status is replied.
The current contact input status is replied.
(C) Alarm
As for the measurement elements set at the main body, “Alarm” will be displayed.
The shift to the test mode needs the setting at the main body.
The upper system cannot shift to the test mode.
- Product Name
- Electronic Multi-Measuring Instrument
- Series
- ME96SS series
May I have your opinion?
Related FAQ
- Connectable number of MODBUS RTU (ME96SS series).
- LCD COM is flashing (ME96SS series).
- Indication values of the main body is different from an obtained value through MODBUS RTU/ TCP (ME96SS series).
- Active energy (lower digit indication) display upon communication test of MODBUS RTU/TCP communication (ME96SS series).
- Availability for battery exchange for Logging Unit (ME96SS series).