FAQ
FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Power Management Meters > Electrical Indicators > LCD COM is flashing (ME96SS series).
FAQ
LCD COM is flashing (ME96SS series).
The COM of the LCD is flashing.
What does it that [COM] in the LCD screen is blinking mean?
What does it that [COM] in the LCD screen is blinking mean?
Answer
A reason varies with the connection situation of options. (Please refer to the section 6 of the User’s Manual.)
In case of MODBUS RTU
Error content: Communication error such as an address error
Please refer to the User’s Manual for error codes and error contents.
Countermeasure: Check the register addresses, function code and the communication settings.
If the correct query received, [COM] is lit.
Error content: Communication error such as an address error
Please refer to the User’s Manual for error codes and error contents.
Countermeasure: Check the register addresses, function code and the communication settings.
If the correct query received, [COM] is lit.
In case of MODBUS TCP (ME-0000MT-SS96)
Error content: Communication error such as a data error of the TCP header part and an address error
Please refer to Section 6 of the “LSPM0075” for error codes and error contents.
Countermeasure: Check the data of the header part and the communication settings.
If the correct query received, [COM] is lit.
Error content: Communication error such as a data error of the TCP header part and an address error
Please refer to Section 6 of the “LSPM0075” for error codes and error contents.
Countermeasure: Check the data of the header part and the communication settings.
If the correct query received, [COM] is lit.
In case of CC-Link (ME-0040C-SS96)
Error content: Hardware error
Countermeasure: Check the wiring between the main body of ME96 and the option.
Error content: Hardware error
Countermeasure: Check the wiring between the main body of ME96 and the option.
In case of Logging unit (ME-0000BU-SS96)
Error content: Setting error, SD memory card error, battery voltage reduction, etc.
Check the LED situation of the option. Please refer to Section 1 of the User’s Manual.
Countermeasure: Refer to Section 1 of the User’s Manual.
Error content: Setting error, SD memory card error, battery voltage reduction, etc.
Check the LED situation of the option. Please refer to Section 1 of the User’s Manual.
Countermeasure: Refer to Section 1 of the User’s Manual.
- Product Name
- Electronic Multi-Measuring Instrument
- Series
- ME96SS series
May I have your opinion?
Related FAQ
- Concurrent-use of MODBUS RTU and CC-Link.
- Active energy (lower digit indication) display upon communication test of MODBUS RTU/TCP communication (ME96SS series).
- Connectable number of MODBUS RTU (ME96SS series).
- Availability for battery exchange for Logging Unit (ME96SS series).
- Indication values of the main body is different from an obtained value through MODBUS RTU/ TCP (ME96SS series).