FAQ


FAQAbout Products
 - FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Input wiring (FX3 series)
 
FAQ
Input wiring (FX3 series)
      Input terminals of the FX3 series are wired and the "X0" terminal and the "0V" terminal are short-circuited. However, the input does not turn on.
    
  
Answer
    For the sink input, the "S/S" terminal and the "24V" terminal are needed to be short-circuited.
  
    - Product Name
 - FX3S, FX3G, FX3GC, FX3U, FX3UC
 
- Product Category
 - Main unit, I/O Extension
 
- Series
 - FX3S, FX3G, FX3GC, FX3U, FX3UC