FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > How to install a battery to FX3G/FX3GC series
FAQ
How to install a battery to FX3G/FX3GC series
I would like to install an optional battery to the FX3G/FX3GC series.
Answer
The FX3U-32BL can be installed to the FX3G/FX3GC series.
After installation, select [Battery Mode: Use the battery] on the FX parameter window of GX Developer or GX Works2.
Please refer to the following manual for further details;
FX3G SERIES PROGRAMMABLE CONTROLLERS USER'S MANUAL(Hardware Edition)
9.3.2 Setting the battery mode
FX3GC SERIES PROGRAMMABLE CONTROLLERS USER'S MANUAL(Hardware Edition)
9.3.2 Setting the battery mode
After installation, select [Battery Mode: Use the battery] on the FX parameter window of GX Developer or GX Works2.
Please refer to the following manual for further details;
FX3G SERIES PROGRAMMABLE CONTROLLERS USER'S MANUAL(Hardware Edition)
9.3.2 Setting the battery mode
FX3GC SERIES PROGRAMMABLE CONTROLLERS USER'S MANUAL(Hardware Edition)
9.3.2 Setting the battery mode
- Product Name
- FX3G, FX3GC
- Product Category
- Main Unit, Accessories, Options
- Series
- FX3G, FX3GC