FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Screen gesture mode and overlap window display
FAQ
Screen gesture mode and overlap window display
What happens to overlap windows when the mode is switched to screen gesture mode while an overlap window is displayed?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
Answer
If the mode is switched to screen gesture mode while an overlap window is displayed, the overlap window is hidden.
The overlap window is redisplayed when screen gesture mode is disabled.
Note that in screen gesture mode, the screen switching device of the overlap windows retains the screen number of the overlap window displayed before the mode was switched to screen gesture mode.
* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture), GOT function (standard function)
- Series
- GOT2000 Series, GOT3000 Series