FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Gesture functions available for the historical trend graph
FAQ
Gesture functions available for the historical trend graph
What gestures are available for the historical trend graph?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
Answer
The following gestures are available for the historical trend graph.
• Swipe in the direction of the time axis: Scrolls the half the page in the swiped direction.*1
• Pinch-in in the direction of the time axis: Zooms out on the time axis by one step (Key code switch equivalent to FFF9)*2
• Pinch-out in the direction of the time axis: Zooms in on the time axis by one step (Key code switch equivalent to FFF8)*2
*1: Zooming in and out on the scale of the device value (vertical axis) with gestures is not supported.
*2: For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture), GOT function (historical trend graph)
- Series
- GOT2000 Series, GOT3000 Series