Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23460
  • Release Date : 2018/09/14 15:06
  • Update : 2025/10/09 18:03
  • Print

Enabling/disabling single touch operation for the historical data list display with a device value

Answer

Even when single touch operation is enabled in the historical data list display settings, you can enable and disable the operation with the device value (GS1794).

When b1 of Gesture Common Control (GS1794) is on: Single touch operation is disabled. 
When b1 of Gesture Common Control (GS1794) is off: Single touch operation is enabled.

Note that when single touch operation is disabled in the historical data list display settings, this signal does not work.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (standard function)
Series
GOT2000 Series, GOT3000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries