FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Range of the screen enlarged with the screen gesture function
FAQ
Range of the screen enlarged with the screen gesture function
How can I determine which part of the original screen is currently displayed on the screen enlarged with the screen gesture function?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
Answer
When screen gesture mode is enabled, a frame indicating the screen gesture active area is displayed.
This frame is displayed with a bright red line only when the contents within the screen gesture active area are not enlarged, and with a combination of bright red and dark red lines when the contents are enlarged. The length and position of the bright red line of the frame indicates which area of the original screen (100%) is being enlarged.

* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture)
- Series
- GOT2000 Series, GOT3000 Series