FAQ


FAQAbout Products
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDSCPU > Battery error
FAQ
Battery error
What devices in the Motion CPU are for battery errors?
- Category :
-
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDSCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MSCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MCPU
Answer
The following shows the devices for the battery errors.
• [SM51] Battery low latch
Turn ON when the voltage of battery reduces to less than 2.5[V].
Remains ON even if the condition is restored to normal thereafter.
• [SM52] Battery low
Turn ON when the voltage of battery reduces to less than 2.5[V].
Turn OFF when the voltage of external battery returns to normal.
• [SM58] Battery low warning latch
Turn ON when the voltage of battery reduces to less than 2.7[V].
Remains ON even if the condition is restored to normal thereafter.
• [SM59] Battery low warning
Turn ON when the voltage of battery reduces to less than 2.7[V].
Turn OFF when the voltage of external battery returns to normal.
• [SM51] Battery low latch
Turn ON when the voltage of battery reduces to less than 2.5[V].
Remains ON even if the condition is restored to normal thereafter.
• [SM52] Battery low
Turn ON when the voltage of battery reduces to less than 2.5[V].
Turn OFF when the voltage of external battery returns to normal.
• [SM58] Battery low warning latch
Turn ON when the voltage of battery reduces to less than 2.7[V].
Remains ON even if the condition is restored to normal thereafter.
• [SM59] Battery low warning
Turn ON when the voltage of battery reduces to less than 2.7[V].
Turn OFF when the voltage of external battery returns to normal.
- Product Name
- Motion controller
- Series
- MELSEC-Q