FAQ


FAQAbout Products
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MSCPU > CUP type of stand-alone Motion controller
FAQ
CUP type of stand-alone Motion controller
What PLC CPU specification is equivalent to that of the stand- alone Motion controller?
- Category :
Answer
The following shows the specification for the PLC CPU area.
Q170MSCPU: Equivalent to PLC CPU "Q03UDCPU"
• Program capacity: 30k steps
• LD instruction processing speed: 0.02μs
Q170MSCPU-S1: Equivalent to PLC CPU "Q06UDHCPU"
• Program capacity: 60k steps
• LD instruction processing speed 0.0095μs
Q170MCPU: Equivalent to PLC CPU "Q03UDCPU" I53 Program capacity: 20k steps
• LD instruction processing speed 0.02μs
Q170MSCPU: Equivalent to PLC CPU "Q03UDCPU"
• Program capacity: 30k steps
• LD instruction processing speed: 0.02μs
Q170MSCPU-S1: Equivalent to PLC CPU "Q06UDHCPU"
• Program capacity: 60k steps
• LD instruction processing speed 0.0095μs
Q170MCPU: Equivalent to PLC CPU "Q03UDCPU" I53 Program capacity: 20k steps
• LD instruction processing speed 0.02μs
- Product Name
- Motion controller
- Series
- MELSEC-Q