Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 38040
  • Release Date : 2021/02/25 17:54
  • Print

EcoWebServerIII's rated voltage value setting with VT connections

When VT is used to input voltage values of measuring devices, which voltage value should be set on the primary or secondary of the VT when setting the EcoWebServerIII of the VT connection device?
Category : 

Answer

For 3P4W circuits, set the VT primary voltage value (between L and N).
Except for 3P4W circuits, set the VT primary voltage value (between L and L).
<Reference> CT: Also sets the primary current value in the same way.
Product Name
Energy Saving Data Collecting Servers, Energy Measuring Units
Series
EcoWebServerIII, EcoMonitorPlus
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?