FAQ


FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Saving Data Collecting Servers > EcoWebServerIII's rated voltage value setting with VT connections
FAQ
EcoWebServerIII's rated voltage value setting with VT connections
When VT is used to input voltage values of measuring devices, which voltage value should be set on the primary or secondary of the VT when setting the EcoWebServerIII of the VT connection device?
Answer
For 3P4W circuits, set the VT primary voltage value (between L and N).
Except for 3P4W circuits, set the VT primary voltage value (between L and L).
<Reference> CT: Also sets the primary current value in the same way.
Except for 3P4W circuits, set the VT primary voltage value (between L and L).
<Reference> CT: Also sets the primary current value in the same way.
- Product Name
- Energy Saving Data Collecting Servers, Energy Measuring Units
- Series
- EcoWebServerIII, EcoMonitorPlus