Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 38041
  • Release Date : 2021/02/25 17:54
  • Print

Pulse magnification setting of EMU4-PX4(Pulse Input Unit)

How to set the pulse conversion rate of EMU4-PX4(Pulse Input Unit) and the pulse factor of EcoWebServerIII? Also, how to deal with one-cycle operation(when the value exceeds the data range and returns to 0)?
Category : 

Answer

Match the setting values with EMU4-PX4 and EcoWebServerIII.
No need to consider one-cycle operation because it is automatically calculated in EcoWebServerIII.
Product Name
Energy Saving Data Collecting Servers, Energy Measuring Units
Series
EcoWebServerIII, EcoMonitorPlus
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?