Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 38042
  • Release Date : 2021/02/25 17:54
  • Print

How to measure circuits over 600A (EcoMonitorPlus / Light)

How to measure circuits over 600A with an Energy Measuring Unit (EcoMonitorPlus / Light)?
Category : 

Answer

As shown in the figure below, a current transformer (CT) with a secondary current of 5A is attached to the measurement location, and a split-type current sensor for the Energy Measuring Unit (model name: EMU-CT5-A, EMU2-CT5, EMU2-CT5-4W) is installed on the secondary side of the CT.
Product Name
Energy Measuring Units
Series
EcoMonitorPlus, EcoMonitorLight
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?