FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > How to measure circuits over 600A (EcoMonitorPlus / Light)
FAQ
How to measure circuits over 600A (EcoMonitorPlus / Light)
How to measure circuits over 600A with an Energy Measuring Unit (EcoMonitorPlus / Light)?
Answer
As shown in the figure below, a current transformer (CT) with a secondary current of 5A is attached to the measurement location, and a split-type current sensor for the Energy Measuring Unit (model name: EMU-CT5-A, EMU2-CT5, EMU2-CT5-4W) is installed on the secondary side of the CT.
![](/usr/file/attachment/dJEFlS9kPaXCoUhu.png)
![](/usr/file/attachment/uVNyO2kMvk0MTo3F.png)
- Product Name
- Energy Measuring Units
- Series
- EcoMonitorPlus, EcoMonitorLight