Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 38042
  • Release Date : 2021/02/25 17:54
  • Print

How to measure circuits over 600A (EcoMonitorPlus / Light)

How to measure circuits over 600A with an Energy Measuring Unit (EcoMonitorPlus / Light)?
Category : 

Answer

As shown in the figure below, a current transformer (CT) with a secondary current of 5A is attached to the measurement location, and a split-type current sensor for the Energy Measuring Unit (model name: EMU-CT5-A, EMU2-CT5, EMU2-CT5-4W) is installed on the secondary side of the CT.
Product Name
Energy Measuring Units
Series
EcoMonitorPlus, EcoMonitorLight

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries