FAQ


FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Saving Data Collecting Servers > Checking the disconnection or communications error status of the Energy measuring Unit
FAQ
Checking the disconnection or communications error status of the Energy measuring Unit
Disconnection or communications error of the Energy Measuring Units connected to EcoWebServerIII can be detected?
Answer
There is no way to detect a disconnection or communications error in the Energy measuring Unit.
As an alternative idea, we have two solutions to monitor the measuring points.
As an alternative idea, we have two solutions to monitor the measuring points.
Solution 1: Having the measuring error information by contact outputs
By setting "Measuring Error" for the contact output conditions, you can find out that the measuring error occurred by contact outputs when you cannot collect measuring point data.
For the procedures, please refer to the User's manual 4.9.3. contact output settings.
By setting "Measuring Error" for the contact output conditions, you can find out that the measuring error occurred by contact outputs when you cannot collect measuring point data.
For the procedures, please refer to the User's manual 4.9.3. contact output settings.
Solution 2: Having the measuring error information by email notifications
By setting "Measuring Error" for the email notifications conditions, you can find out that the measuring error occurred by email notifications.
For the procedures, please refer to the User's manual 4.9.6. EcoWebServerIII error notification settings.
By setting "Measuring Error" for the email notifications conditions, you can find out that the measuring error occurred by email notifications.
For the procedures, please refer to the User's manual 4.9.6. EcoWebServerIII error notification settings.
- Product Name
- Energy Saving Data Collecting Servers
- Series
- EcoWebServerIII