FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding understanding the difference between "Batch Setting of PDO Mapping" and "PDO Mapping Setting".
FAQ
Regarding understanding the difference between "Batch Setting of PDO Mapping" and "PDO Mapping Setting".
What is the difference between setting up "Batch Setting of PDO Mapping" or "PDO Mapping Setting"?
Answer
The batch setting of PDO mapping sets the default PDO mapping for all device stations that support PDO mapping.
*Note that in the batch setting of PDO mapping, the 1st mapping pattern which is not supported by FX5-CCLGN-MS is set.
*Note that in the batch setting of PDO mapping, the 1st mapping pattern which is not supported by FX5-CCLGN-MS is set.
The PDO mapping configuration sets the PDO mapping for each device station that supports PDO mapping.
See the manual below.
MELSEC iQ-F FX5 CC-Link IE TSN Master/Local Module User's Manual
MELSEC iQ-F FX5 CC-Link IE TSN Master/Local Module User's Manual
- Product Name
- FX5-CCLGN-MS
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series