FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding how to compare multiple word devices
FAQ
Regarding how to compare multiple word devices
Is there a way to compare multiple word devices?
Answer
It is possible to compare multiple word devices using the BKCMP_□ instruction.
*where □ is the comparison symbol.
Example:To compare 10 stores from D0 to D9 and from D100 to D109, write [BKCMP _□ D0 D100 D200 K10].
Comparison result is stored in 10 points from D200.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module
- Series
- MELSEC iQ-F Series