FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding replacement from 128 point type of FX3U
FAQ
Regarding replacement from 128 point type of FX3U
I am considering replacing the FX3U-128MR/ES, but the FX5U CPU module is limited to a 80 point lineup, so what kind of configuration should I make?
Answer
The FX5U CPU module has a lineup of up to 80 point.
The following configuration is recommended when replacing the FX3U-128MR/ES.
Recommended alternative (1)
・FX5U-80MR/ES + FX5-32ER/ES + FX5-16ER/ES
Recommended alternative (2)
・FX5UJ-60MR/ES + FX5-32ER/ES + FX5-32ER/ES + FX5-8EYR/ES
- Product Name
- FX5U, FX5UC, FX5UJ
- Product Category
- CPU Module
- Series
- MELSEC iQ-F Series