Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 44873
  • Release Date : 2025/03/18 10:23
  • Print

Regarding whether ladder monitoring is enabled by the Web server function

Is it possible to monitor the ladder with the web server function? If not, what can be monitored using the Web Server function?

Category : 

Answer

You cannot use the ladder monitor with the Web server function. 

With the Web server function, it is possible to monitor the device value, test the device (writing an arbitrary value to the device), diagnose the CPU, check the access log (Access logs, operation details, and access source IP address), and check the event history (event occurrence date and time).

Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries