FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Automation Controllers MELSEC > MELSEC MX Controller MX-F Model > Regarding the built-in motion function
FAQ
Regarding the built-in motion function
What is the difference between the built-in motion function of the MX-F Model and the FX5 -40/80SSC-G of the iQ-F series?
Answer
The built-in motion function of the MX-F Model is programmed using motion control FB, wheareas the FX5-40/80SSC-G of the iQ-F series is programmed using buffer memory.
Also, the supported functions are different, and the Technical bulletin below describes the functional differences.
[Technical bulletin]
・Differences Between MELSEC iQ-F Series And MELSEC MX Controller MX-F Model<FAM-A-0102-A>
- Product Name
- MX-F Model
- Series
- MELSEC MX Controller