FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Automation Controllers MELSEC > MELSEC MX Controller MX-F Model > Regarding number of internal Ethernet port connections
FAQ
Regarding number of internal Ethernet port connections
How many connections does the built-in Ethernet port (P2) on the MX-F Model have?
Answer
The Ethernet port (P2) has 32 connections.
The breakdown is as follows: total of MELSOFT connections, SLMP, and socket communications ≦ 32 connections.
Apart from the above, one connection is supported for FTP.
- Product Name
- MX-F Model
- Series
- MELSEC MX Controller