FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Automation Controllers MELSEC > MELSEC MX Controller MX-F Model > Regarding the built-in positioning function
FAQ
Regarding the built-in positioning function
The CPU Module of the iQ-F series supports the built-in positioning function, but does the MX-F Model also support it?
Answer
The MX-F Model also supports the built-in positioning function.
The number of control axes is now 4, and PULSE/SIGN and CW/CCW are supported.
The maximum frequency is 200kpps.
- Product Name
- MX-F Model
- Series
- MELSEC MX Controller