FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Closing the window screen
FAQ
Closing the window screen
How do I close the window screen?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > Engineering Software
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT2000
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > Engineering Software > HMI/GOT Screen Design Software
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT3000
Answer
The following three methods are available to close the window screen.
1. Touch the [x] button on the right side of the title bar displayed on the window screen.
* This function cannot be used when the title bar is hidden.
2. Close the window screen with the touch switch
The following shows how to close the window screen (overlap window, superimpose window, or dialog window) using the touch switch.
Set the touch switch using the screen design software.
◆ For GT Designer3 (GOT2000) Version 1
(1) Place a touch switch on the screen.
(2) Double-click the placed touch switch to display the [Switch] dialog.
(3) Select [Screen Switching] in the [Action] tab.
(4) Select the screen to be closed for [Screen Type], select [Fixed] for [Next Screen], then set "0" for [Screen No.].
3. Write "0" to the screen switching device.
The window screen will close once "0" is written to screen switching device of the window screen (overlap window, superimpose window, or dialog window).
◆ For GT Designer3 (GOT2000) Version 1
The number to close the window screen can be set to a value other than 0.
Change the setting in GT Designer3.
[Common] - [GOT Environmental Setting] - [Screen Switching/Windows] - [Other Setting] - [Screen No. of the window screen to be hidden]
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (standard function)
- Series
- GOT2000 Series, GOT Screen Design Software, SoftGOT2000, GOT3000 Series, SoftGOT3000