FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > How to export the alarm data stored on the GOT to a personal computer
FAQ
How to export the alarm data stored on the GOT to a personal computer
How do I export the alarm data stored on the GOT to a personal computer?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT2000
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GT SoftGOT > SoftGOT3000
Answer
The following methods are available for exporting the alarm data stored on the GOT to a personal computer.
1. Export the data using the resource data transfer function of the screen design software.
2. Export the data using the Data Transfer Tool.
3. Write the alarm data on the GOT to the data storage (USB memory or SD memory card) to export the data.
4. Access the alarm data using the FTP server function or the FTP client function.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (alarm)
- Series
- GOT2000 Series, SoftGOT2000, GOT3000 Series, SoftGOT3000